• No : 21783
  • Release Date : 2018/08/22 16:29
  • Print

Setting frequency

When using the inverter in the external operation mode, the frequency setting value set by the external potentiometer is not output until the inverter operates. Therefore, I cannot confirm while setting it.
I want to check the setting frequency while the inverter is stopped.
Category : 

Answer

Set Pr.52 (DU/PU main display data selection) to "100".
Displaying the setting frequency while the inverter is stopped and the output frequency while it is operating on the monitor.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700