- No : 21783
- Release Date : 2018/08/22 16:29
-
Print
Setting frequency
When using the inverter in the external operation mode, the frequency setting value set by the external potentiometer is not output until the inverter operates. Therefore, I cannot confirm while setting it.
I want to check the setting frequency while the inverter is stopped.
- Category :
-
Answer
Set Pr.52 (DU/PU main display data selection) to "100".
Displaying the setting frequency while the inverter is stopped and the output frequency while it is operating on the monitor.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700