- No : 21784
- Release Date : 2018/08/22 16:29
-
Print
Setting frequency
I want to continuously display the setting frequency of the inverter.
I want to display the setting frequency also when the inverter is powered on.
- Category :
-
Answer
Set Pr.52 (DU/PU main display data selection) to "5".
This allows for displaying the setting frequency on the voltage monitor.
Then, switch to the monitor mode and press the "SET" key twice to display the setting frequency ("Hz" on the monitor flickers). Press and hold the "SET" key for a while to change the initial display upon power-on to setting frequency. (First monitored window)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700