- No : 21794
- Release Date : 2018/08/22 16:29
-
Print
Frequency setting
I use an external potentiometer to give frequency commands. What happens if the frequency commands from the potentiometer cease?
- Category :
-
Answer
When the potentiometer is disconnected and frequency commands cease, the input potential becomes around 0 V.
Therefore, the frequency command becomes analog-calibrated frequency around 0 V.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700