- No : 21796
- Release Date : 2018/08/22 16:29
-
Print
Frequency setting
I use Speed 15 of the multi-speed setting. Can I set the frequencies randomly instead of setting them in the order of low, middle, and high speeds?
- Category :
-
Answer
Yes, you can set them randomly.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700