- No : 21798
- Release Date : 2018/08/22 16:29
-
Print
Frequency setting
Is it necessary to set parameters to change the frequency during PU operation?
- Category :
-
Answer
No.
Just turn the setting dial to select a frequency and press the "SET" key, and the inverter operates at the selected frequency.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700