- No : 21804
- Release Date : 2018/08/22 16:29
-
Print
Frequency setting
I want to operate the inverter in the JOG mode by short-circuiting externally assigned terminals JOG and SD and setting the frequency with an external potentiometer.
- Category :
-
Answer
In this case, the JOG operation is prioritized.
When the terminals JOG and SD are short-circuited and turned ON, the frequency setting by the external potentiometer is ignored and invalid.
To use the external potentiometer, turn OFF the terminals JOG and SD.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700