• No : 21809
  • Release Date : 2018/08/22 16:29
  • Print

Frequency manual controller FR-AX

What is the maximum wiring length between the frequency manual controller FR-AX (with the frequency setting potentiometer, start switch, and frequency meter) and the inverter?  
Category : 

Answer

Considering voltage drop of the internal power supply and influence by noise, the wiring length should be 30 m or less.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700