- No : 21809
- Release Date : 2018/08/22 16:29
-
Print
Frequency manual controller FR-AX
What is the maximum wiring length between the frequency manual controller FR-AX (with the frequency setting potentiometer, start switch, and frequency meter) and the inverter?
- Category :
-
Answer
Considering voltage drop of the internal power supply and influence by noise, the wiring length should be 30 m or less.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700