- No : 21814
- Release Date : 2018/08/22 16:29
-
Print
Base frequency setting value
What value should I set the base frequency to?
- Category :
-
Answer
Set the rated frequency of the motor used to it.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700