- No : 21817
- Release Date : 2018/08/22 16:29
-
Print
External installation<br>Rated current
Where should I install the external thermal?
What is the rated current?
- Category :
-
Answer
Since the external thermal prevents the motor from being overheated, install it between the output terminal of the inverter and the motor.
The rated current is the maximum current value that can continuously and safely flow through the inverter.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700