- No : 21825
- Release Date : 2018/08/22 16:29
-
Print
CC-Link
In CC-Link operation, is it possible to set the running frequency continuously?
- Category :
-
Answer
Yes. However, write the setting data to the RAM of the inverter.
Set RWw1 in the setting value and turn ON the frequency setting command RYD.
To continuously set the frequency, keep the command RYD turned ON.
The setting completion RXD turns ON when writing completes. You can ignore it.
Note that if Pr.544 (CC-Link extended setting) is set to "0", when RYD and RYE turn ON simultaneously, RYD is prioritized.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700