• No : 21844
  • Release Date : 2018/08/22 16:29
  • Print

Control terminal

Can I use the inverter by connecting the terminals STF and SD and by setting the frequency using the setting dial?
Category : 

Answer

You also need to set Pr.79 (Operation mode) to "3".
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700