- No : 21844
- Release Date : 2018/08/22 16:29
-
Print
Control terminal
Can I use the inverter by connecting the terminals STF and SD and by setting the frequency using the setting dial?
- Category :
-
Answer
You also need to set Pr.79 (Operation mode) to "3".
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700