• No : 21848
  • Release Date : 2018/08/22 16:29
  • Print

Frequency setting

Answer

When using the setting dial to set the frequency, turn the dial and display the frequency. Then, press the "SET" key while the desired value flickers.
The frequency is not set unless you press the "SET" key.
You can also set the potentiometer mode that does not require pressing the "SET" key but turning it to change the frequency. (Set Pr.161 to "1".)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700