- No : 21865
- Release Date : 2018/08/22 16:29
-
Print
Terminal FM
I want to use the ammeter connected to the terminal FM so that the output current monitor 10 A becomes the full scale.
- Category :
-
Answer
Set Pr.56 (Current monitor reference) to "10A".
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700