- No : 21866
- Release Date : 2018/08/22 16:29
-
Print
Frequency setting
The terminal FM indicates that the full scale is 0 to 1 mA. Does the frequency indication become the full scale at 60 Hz operation?
- Category :
-
Answer
The full scale of the frequency is initially set to 60 Hz and the frequency indication becomes the full scale at 60 Hz operation.
To change the indication value, change Pr.55 (Frequency monitor reference) to the new full scale value.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700