- No : 21868
- Release Date : 2018/08/22 16:29
- 
          
              Print
          
        
 
CC-Link
    
      The Instruction Manual of the FR-A7NC instructs not to create an empty station number. Does this mean I should create reserved stations?  
    
  
    - Category : 
- 
      
    
 
    Answer
  
    It is OK if stations are set as reserved.
  
    
      
        - Product Name
- Inverter, magnet motor drive
        - Product Category
- Inverter
        - Series
- FR-E700, FR-A700, FR-F700P, FR-F700