• No : 21868
  • Release Date : 2018/08/22 16:29
  • Print

CC-Link

The Instruction Manual of the FR-A7NC instructs not to create an empty station number. Does this mean I should create reserved stations?  
Category : 

Answer

It is OK if stations are set as reserved.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700, FR-F700P, FR-F700