- No : 21885
- Release Date : 2018/08/22 16:29
-
Print
CC-Link
I cannot find explanation on how to monitor power in the Instruction Manual of the FR-A7NC. Is it possible?
What is the unit of power output?
- Category :
-
Answer
You can select from the output power (in 0.01 kW units) and cumulative energy (in 1 kWh/0.01 kWh units).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700