- No : 21903
 
      - Release Date : 2018/08/22 16:30
 
        - 
          
              Print
          
        
 
  
 
CC-Link
    
      I connected the inverter via CC-Link but the "NET" LED on the inverter's operation panel does not turn on.
How can I turn it on?
    
  
    - Category : 
 
    - 
      
    
 
  
 
    Answer
  
    Set Pr.340 (Communication startup mode selection) to other than "0".
Also, set Pr.79 (Operation mode) to "0", "2", or "6".
Powering the inverter on automatically puts it in the NET mode and "NET" on the operation panel turns on.
  
    
      
        - Product Name
 
          - Inverter, magnet motor drive
 
      
      
        - Product Category
 
          - Inverter
 
      
      
        - Series
 
          - FR-E700, FR-A700, FR-F700P, FR-F700