- No : 21905
- Release Date : 2018/08/22 16:30
-
Print
CC-Link
I am considering to use the CC-Link option for CC-Link communication.
The Instruction Manual instructs to set consecutive numbers for the station numbers. Can I set reserved stations?
- Category :
-
Answer
You can set reserved and invalid stations.
The Instruction Manual instructs to set consecutive numbers because the master regards an empty number as an error.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700