• No : 21906
  • Release Date : 2018/08/22 16:30
  • Print

NET mode, external operation switching

I want to use the inverter normally in CC-Link operation and occasionally connect to an external frequency setting potentiometer (WA2W, 1 kΩ) to set the frequency.
Can I switch between the NET mode and external operation?
Which parameter should I set for this purpose?
Category : 

Answer

You can switch between the NET mode and external operation.
Assign the X66 signal (Operation switching) to an unused terminal for switching.
Also, set Pr.79 (Operation mode) to "6".
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700, FR-F700P, FR-F700