- No : 21912
- Release Date : 2018/08/22 16:30
-
Print
Frequency setting
Does using a frequency setting potentiometer of 2 kΩ affect inverter operation?
- Category :
-
Answer
You can use it for inverter operation, but the running speed of the inverter does not change linearly with regard to turn of the frequency setting potentiometer.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700