• No : 21913
  • Release Date : 2018/08/22 16:30
  • Print

Frequency setting

Which parameter should be used to set the maximum value using the externally connected frequency setting potentiometer?
Category : 

Answer

Use Pr.125 (Terminal 2 frequency setting gain frequency). 
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700