- No : 21914
- Release Date : 2018/08/22 16:30
-
Print
FR-Configurator
Can I use the FR Configurator FR-SW3-SETUP-WJ to operate the inverter?
- Category :
-
Answer
The FR Configurator FR-SW3-SETUP-WJ can only allow for test operation.
Since this is a tool to support the system launch and maintenance, it is not designed for actual operation.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700