- No : 21919
- Release Date : 2018/08/22 16:30
-
Print
FR-PU04
I want to use the FR-PU04 used with the 500 series with the 700 series.
Can I set parameters that were not used with the 500 series by the FR-PU04?
- Category :
-
Answer
While the FR-PU04 does not display parameter names, it displays parameter numbers and you can set them.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700