- No : 23562
- Release Date : 2018/09/14 15:09
-
Print
Major error 093CH
What is major error 093CH?
What should I do when it occurs?
- Category :
-
Answer
Major error 093CH occurs when the absolute position is erased.
Execute the home position return after checking the batteries of the Motion CPU module and the servo amplifier.
- Product Name
- Motion controller
- Series
- MELSEC iQ-R