FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Setting value of Pr.72 (FR-B, B3 (A800 base))
FAQ
Setting value of Pr.72 (FR-B, B3 (A800 base))
Pr.72 (PWM frequency selection) cannot be set. What is the setting value?
- Category :
Answer
For the normal type (FR-B3) is 2 KHz. For the low-noise type (FR-B3-N), 14.5 KHz.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-B/B3(A800)