FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Trace function
FAQ
Trace function
When the data is acquired in the record mode of the trace function, two files, ST1 and TR1, are saved. What are these files?
- Category :
Answer
The ST1 is a setting file and the TR1 is a waveform file.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800