Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21052
  • Release Date : 2018/08/22 16:25
  • Print

Terminal block

Are the specifications of the main circuit terminals of the FR-A800, FR-F800, and FR-D700 the same? Is the same cable gauge available?
Category : 

Answer

The specifications are the same. The same cable gauge is available.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800, FR-D700, FR-E700, FR-E700, FR-F700PJ

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries