FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Orientation control
FAQ
Orientation control
After the X22 signal is turned ON, the motor keeps rotating at the speed of the setting value of Pr.351 (Orientation speed). What is the possible cause?
- Category :
Answer
The following reasons are possible.
- The signal of Z phase does not exist. (It is not returned normally.)
- The setting of Pr.359 encoder rotation direction is reversed.
- The setting of Pr.369 number of encoder pulses is not correct.
- The signal of Z phase does not exist. (It is not returned normally.)
- The setting of Pr.359 encoder rotation direction is reversed.
- The setting of Pr.369 number of encoder pulses is not correct.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700