FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > ABC terminal
FAQ
ABC terminal
Can the ABC relay (error) output be conductive in normal, not conductive when powered OFF, and not conductive at an error occurrence?
- Category :
Answer
It is possible by using the terminal A to C with the negative logic setting.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700