FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Remote setting function
FAQ
Remote setting function
In the Instruction Manual, it is described that "The remote setting function is disabled during JOG operation and PID control operation". Does the multi-speed function operate during JOG operation (or during PID control operation) with Pr.59 (Remote function selection) set 1 to 3?
- Category :
Answer
Because the multi-speed terminal is disabled, it does not operate in multi-speed.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700