FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Parameter copy
FAQ
Parameter copy
It is described that parameter copy in the FR-A700 and FR-F700(P) with the DU07 should be performed while the inverter is stopped. What happens if it is performed during the operation?
- Category :
Answer
Reading during the operation is possible. However, when writing is performed during the operation, "rE2" (parameter write error) occurs.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700, FR-F700P, FR-F700