FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Remote input signal of CC-Link communication
FAQ
Remote input signal of CC-Link communication
Is the remote input signal (RX bit) sent from the inverter (FR-A7NC) to master module retained when the communication error (E.OP1, E.OP3) occurs?
- Category :
Answer
When the communication error occurs, the input signal status is not retained, and all the bits turn OFF. When the communication establishes again, the bit turns ON/OFF even if the alarm occurs in the inverter.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700