FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Noise filter
FAQ
Noise filter
Is the noise filter built-in the FR-E700 series?
- Category :
Answer
The noise filter is not built-in the FR-E700 series.
It is built in the FR-A700/F700 series with the 55K or lower capacity.
It is built in the FR-A700/F700 series with the 55K or lower capacity.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700