FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Remote operation of the inverter
FAQ
Remote operation of the inverter
I want to perform remote operation of the inverter with the different enclosure contact. How long can I extend the control circuit and input signal (contact) circuit? (Example: 100 m etc.)Also, what is the voltage of this circuit?
- Category :
Answer
The wiring length of the start signal (STF etc.) is 30 m or less.
The circuit voltage of the control input signals (terminal STF etc.) is 24 VDC and the voltage when contacts are open is from 21 to 27 VDC.
The circuit voltage of the control input signals (terminal STF etc.) is 24 VDC and the voltage when contacts are open is from 21 to 27 VDC.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A500