FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Torque characteristic at low speed
FAQ
Torque characteristic at low speed
The catalog indicates the speed control range without PG as 1:120 (0.5 Hz to 60 Hz power driving).
What are the speed fluctuation rate and torque characteristics at 0.5 Hz or slower?
What are the speed fluctuation rate and torque characteristics at 0.5 Hz or slower?
- Category :
Answer
Torque is not guaranteed for slower than 0.5 Hz.
Therefore, no data for this is published. Also, no torque is generated at 0 Hz.
Therefore, no data for this is published. Also, no torque is generated at 0 Hz.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A500