FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Drive Products > Inverters-FREQROL > Amount of heat generated
FAQ
Amount of heat generated
How much heat does the vector inverter generate?
- Category :
Answer
The following amount of heat is generated under the 100% load. (The same amount for both the 200 V and 400 V classes.
The amount of heat generated by the built-in brake resistor is not included.)
<<Amount of heat generated by vector inverter>>
- 1.5K ????? 150 W
- 2.2K ????? 240 W
- 3.7K ????? 330 W
- 5.5K ????? 440 W
- 7.5K ????? 670 W
- 11K ????? 860 W
- 15K ????? 1100 W
- 18.5K ????? 1300 W
- 22K ????? 1750 W
- 30K ????? 2100 W
- 37K ????? 2400 W
- 45K ????? 2700 W
The amount of heat generated by the built-in brake resistor is not included.)
<<Amount of heat generated by vector inverter>>
- 1.5K ????? 150 W
- 2.2K ????? 240 W
- 3.7K ????? 330 W
- 5.5K ????? 440 W
- 7.5K ????? 670 W
- 11K ????? 860 W
- 15K ????? 1100 W
- 18.5K ????? 1300 W
- 22K ????? 1750 W
- 30K ????? 2100 W
- 37K ????? 2400 W
- 45K ????? 2700 W
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-V200