FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Key sheet
FAQ
Key sheet
Can I remove the key sheet?
Is there a connector below the key sheet for connecting to the FR-PU03?
Is there a connector below the key sheet for connecting to the FR-PU03?
- Category :
Answer
You cannot remove the key sheet from products with the key sheet attached as a standard other than the PU operation type.
When using the parameter unit FR-PU03, use the PU operation type FR-U100.
The PU operation type does not have the key sheet but a connector instead.
When using the parameter unit FR-PU03, use the PU operation type FR-U100.
The PU operation type does not have the key sheet but a connector instead.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Common
- Series
- FR-U100