Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21628
  • Release Date : 2018/08/22 16:28
  • Print

Compatibility of the function with FR-A100

Are the functions of the FR-A100EXCELLENT and FR-A100 compatible?
Category : 

Answer

Yes.
Compared with the FR-A100:- The PI control function is added.- Fast-response current limit operation is improved.- Cumulative energy monitor is added.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A100

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries