FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Automatic restart after instantaneous power failure
FAQ
Automatic restart after instantaneous power failure
Is it possible to restart the inverter after power failure? (Is automatic restart after instantaneous power failure available?)
- Category :
Answer
The inverter has the automatic restart after instantaneous power failure function.
By setting Pr.61 to other than "9999", the encoder detects the speed of the inverter after the power restores and restarts it from the coasting speed.
By setting Pr.61 to other than "9999", the encoder detects the speed of the inverter after the power restores and restarts it from the coasting speed.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-V200