FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Drive Products > Inverters-FREQROL > Encoder signal output
FAQ
Encoder signal output
Is it possible to output the encoder signal?
- Category :
Answer
It can be output by attaching the plug-in option FR-VPA, FR-VPB, or FR-VPC.
Note that the output format depends on the option type.
FR-VPA: Open collector output (phases A, B, and Z)FR-VPB: Line driver output (phases A, B, and Z)FR-VPC: Line driver output (phases A and B only)Also, note that a divided signal cannot be output.
Note that the output format depends on the option type.
FR-VPA: Open collector output (phases A, B, and Z)FR-VPB: Line driver output (phases A, B, and Z)FR-VPC: Line driver output (phases A and B only)Also, note that a divided signal cannot be output.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-V200