FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Small capacity vector inverter dedicated motor
FAQ
Small capacity vector inverter dedicated motor
Do you have small capacity vector inverter dedicated motors (1.5 to 3.7 kW)?
- Category :
Answer
We offer 5.5 kW or higher SF-VR dedicated motors and do not offer small capacity (3.7 kW or lower) motors.
If you need small capacity (1.5 kW to 3.7 kW), use a motor with an encoder.
If you need small capacity (1.5 kW to 3.7 kW), use a motor with an encoder.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Dedicated motor
- Series
- FR-V200