FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Use of general-purpose servo motor
FAQ
Use of general-purpose servo motor
Can I use a servo motor for general-purpose servo MR-VA?
- Category :
Answer
You can operate it by adjusting the motor constant by the auto tuning function.
(Note that the same characteristics as operated by the servo amplifier MR-VA are not achieved.)
(Note that the same characteristics as operated by the servo amplifier MR-VA are not achieved.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-V200