FAQ


FAQAbout Products
 
 - FAQ > Drive Products > Inverters-FREQROL > Applicable motors
FAQ
Applicable motors
      What types of motors are applicable?
    
  - Category :
Answer
    In addition to the dedicated motor (SF-VR series), the SF-JR series motor with an encoder can be used. 
You can also use a standard motor by combining it with an encoder.
Further, you can use a geared motor by combining it with an encoder and performing auto tuning.
Note that the encoder must be directly linked to the motor shaft.
You can use motors with encoders from other manufacturers by performing auto tuning.
    You can also use a standard motor by combining it with an encoder.
Further, you can use a geared motor by combining it with an encoder and performing auto tuning.
Note that the encoder must be directly linked to the motor shaft.
You can use motors with encoders from other manufacturers by performing auto tuning.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-V200