FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Comparison with FR-A200E
FAQ
Comparison with FR-A200E
What are the differences in functions with the FR-A200E?
- Category :
Answer
In addition to speed control, you can also select torque control as well as you can perform position control using an option.
The speed control range is as large as 1:1500, enabling stable operation at ultra-low speed.
Response is faster.
Many vector control adjustment parameters, such as speed control gain or torque gain, are added.
You can switch between vector control and V/F control.
Two systems of analog signal output are available.
The speed control range is as large as 1:1500, enabling stable operation at ultra-low speed.
Response is faster.
Many vector control adjustment parameters, such as speed control gain or torque gain, are added.
You can switch between vector control and V/F control.
Two systems of analog signal output are available.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-V200