FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Model configuration
FAQ
Model configuration
What types are available?
- Category :
Answer
12 models of FREQROL-V200 vector inverters each for the 200 V and 400 V classes from 1.5K to 45K.
9 models of SF-VR vector control dedicated motors each for the 200 V and 400 V classes from 5.5 to 45K. (55K or higher capacity is supported by the MELTRAC-V200 series.) (55K or higher capacity is supported by the MELTRAC-V200 series.)
9 models of SF-VR vector control dedicated motors each for the 200 V and 400 V classes from 5.5 to 45K. (55K or higher capacity is supported by the MELTRAC-V200 series.) (55K or higher capacity is supported by the MELTRAC-V200 series.)
- Product Name
- Inverter, magnet motor drive
- Series
- FR-V200