FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Advanced magnetic flux vector control
FAQ
Advanced magnetic flux vector control
While using Advanced magnetic flux vector control by setting Pr.80 (Motor capacity) and Pr.81 (Number of motor poles), the monitor frequency fluctuates. Can I eliminate slip compensation?
- Category :
Answer
Yes. Set Pr.89 (Speed control gain) to "0".
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700